Safeties - Verasys - LIT-12013067 - LC-VAC1000-0 - LC-VAC3000-0 - LC-IOM3711-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document type
Application Note
Document number
LIT-12013067
Revision date
2023-04-27

A shutdown procedure activates when a low temperature alarm input is closed. The procedure varies depending on the following two situations:

  • When triggered and proportional heating or cooling is defined, the dampers fully close and the cooling or heating output is set to the failsafe position, and the fan stops.
  • When triggered and no proportional heating or cooling is defined, the dampers fully close and the unit remains operating.