From the menu, you can select staged heating, proportional heating, heat pump, or heat pump with supplemental heat by changing the Heating Device Type parameter. You can also set an outside air temperature high limit from the menu or the menu depending on the heating device type you select. If the outside air rises above this setpoint, the unit prevents heating.