Occupancy mode - Verasys - LIT-12013067 - LC-IOM3711-0 - LC-VAC1000-0 - LC-VAC3000-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document type
Application Note
Document number
LIT-12013067
Revision date
2023-04-27

Setting schedules on the controller defines the occupancy mode. You can also synchronize schedules from the SBH. In the Status menu of the controller, you can override occupancy mode by changing the Occupancy Override. If you override the schedule, the controller disregards the schedule until you reset the Occupancy Override to the Not Set state. From the Status menu on the homepage, you can see the current Occupancy Status.

On the Commissioning menu, in the Setpoints section, if the Heat cool Setpoint Mode is set to Common Setpoint the controller uses the Temperature Setpoint and Deadband to configure setpoints in the occupied state. The Deadband determines the difference between the heating and cooling setpoints. If the Heat cool Mode is set to individual setpoints, Dead band is not displayed and does not apply. Regardless of the Heat Cool Setpoint Mode is selected, the system cools or heats to the Effective Heating and Cooling Setpoints.

In occupied mode, you can enable the Occupancy BI Enabled input in the Details > Sensors section of the menu. If you configure the binary input, the unit expects a contact that results in different outcomes depending on whether or not the contact is made:

  • If the contact occurs, the binary input sets the unit to occupied mode.
  • If the contact does not occur, the binary input sets the unit to standby mode.

Temp Occupancy time does not apply to Occupancy Binary Input. An example of a typical device that you can use as a binary input is a motion sensor or relay connected to a lighting circuit.

If the NS8000 sensor has a PIR occupancy sensor installed, the unit functions in occupied mode regardless of the Occupancy BI Enabled setting.