Load shed - Verasys - LIT-12013067 - LC-VAC1000-0 - LC-VAC3000-0 - LC-IOM3711-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document type
Application Note
Document number
LIT-12013067
Revision date
2023-04-27

Before you begin

You must have a LC-VAC1002-0 or a generic Input Output Module (IOM) with a generic IOM application installed to initiate a load shed command to Verasys. To initiate a load shed command, ensure that BI-2 is a closed contact to the LC-IOM100-0 or LC-VAC1002-0. For more information about configuring the generic IO application for load shed, refer to the Load shedding section of Verasys System User Guide (LIT-12012371) .

About this task

You can set the built-in load shed feature to automatically raise and lower the effective heating and cooling setpoints when triggered. To set the rate and limit of the load shed, complete the following steps:

Procedure

  1. Navigate to the Details menu.
  2. Navigate to the System Configuration section.
  3. Change Load Shed Allowed to Yes.
  4. Navigate to the Commissioning menu.
  5. Navigate to the Load Shed section.
  6. Change the Load Shed Adjust and Load Shed Rate Limit according to your needs.