Humidification control - Verasys - LIT-12013067 - LC-VAC1000-0 - LC-VAC3000-0 - LC-IOM3711-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document type
Application Note
Document number
LIT-12013067
Revision date
2023-04-27
Note: Humidification is possible only when you have extended the controller’s features using LC-IOM3711-0.

To check if a humidity sensor is installed, navigate to Details > Sensors. If a humidity sensor is set to something other than Not Installed, and the Humidity Enable parameter in the System Configuration > Details section is set to Enable, the option for humidification is present. When humidification is present, the unit modulates the humidity output to maintain a humidity setpoint. A humidifier binary output is also energized when a required humidification is present. You must install a humidity high limit transmitter, for example, the P/N HL-67N5-8N00P, in the duct to limit the maximum humidity level discharged by the humidifier.