In the menu, you can select a fixed variable fan for the supply fan type. If selected, the fan modulates with the heating or cooling command. The relationship varies depending on the type of heating and cooling equipment present. In the Fan section of the Commissioning menu, you can configure the fan speed based on the type of heating and cooling equipment.