Data share - Verasys - LIT-12013067 - LC-VAC1000-0 - LC-VAC3000-0 - LC-IOM3711-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document type
Application Note
Document number
LIT-12013067
Revision date
2023-04-27

Data share facilitates the sharing of meaningful data between SMART system components. You can share the following objects using data share:

  • Outdoor Air Temperature
  • Temperature Setpoint
  • Unoccupied Cooling Setpoint
  • Unoccupied Heating Setpoint
  • Standby Cooling Setpoint
  • Standby Heating Setpoint
Note: If you do not have an outside air temperature sensor installed, the controller can share the value from another controller that does have one.