Cooling coil - Verasys - LIT-12013067 - LC-IOM3711-0 - LC-VAC1000-0 - LC-VAC3000-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document type
Application Note
Document number
LIT-12013067
Revision date
2023-04-27

From the Details > System Configuration menu, you can select staged cooling, proportional cooling, or heat pump.

A parameter for outside air temperature low limit locks out the cooling if the outside air falls below a setpoint.