Point to point wiring diagrams - Verasys - LIT-12013067 - LC-VAC1000-0 - LC-VAC3000-0 - LC-IOM3711-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document number
LIT-12013067
Revision date
2023-04-27
Product status
Discontinued

You can expand the features of the LC-VAC1000-0 and the LC-VAC3000-0 when you combine either controller with the LC-IOM3711-0. See the following wiring diagrams for combining both controllers with the LC-IOM3711-0.