Updating the VAC controller firmware - Verasys - LIT-12013067 - LC-IOM3711-0 - LC-VAC1000-0 - LC-VAC3000-0 - Field Device - Verasys Constant Volume Controller
Verasys Constant Volume Controller Application Note
- Product
- Controls > Field Controls > Verasys Constant Volume Controller
- Document type
- Application Note
- Document number
- LIT-12013067
- Revision date
- 2023-04-27
Before you begin
Use separate USB 2.0 drives to store the
application file, clean file, and backup configuration files. Format the USB drives
for the FAT or FAT32 format.
Procedure
-
To back up the VAC configuration .csv files, insert a USB
drive into the USB port on the controller and navigate to . Record the date and time for each LC-VAC1000-0 controller if
you are updating multiple controllers.
-
Download the clean and application package files from the
Partners Portal on http://verasyscontrols.com or request the package files through email at http://be-verasyssupport@jci.com
.
-
If the VAC1000 is connected to the Smart Building Hub, remove
the system bus connection and remove offline devices in the
Devices page. Refer to the Devices
section of the Verasys System User Guide
(LIT-12012371).
-
Download the Clean_VAC1000_xxxx.pkg to
the root folder of a blank USB drive and then download the
CV_App_VAC1000_x.x.x.x.pkg to the root folder of
another blank USB drive.
-
Insert the USB drive with the clean package into the USB
port on the controller.
-
On the controller local display, navigate to
and press Enter.
-
When the clean package finishes and the local display shows
Clean, remove the USB drive.
-
Insert the USB drive with the application package into the USB
port.
-
If the update does not start automatically, navigate to and press Enter.
-
When the application update finishes, navigate to and verify that the version is updated correctly.
-
To restore your backup configuration file, insert the USB
drive with the backup files into the controller, and navigate to . Select the appropriate backup .csv file and press
Enter.
-
Reconnect the system bus to the controller.