Setting the VAC controller address using the local display - Verasys - LIT-12013067 - LC-VAC1000-0 - LC-VAC3000-0 - LC-IOM3711-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document number
LIT-12013067
Revision date
2023-04-27
Product status
Discontinued

Procedure

  1. Press the ENT (Enter) button to access the menu.
  2. Use the up and down arrows to navigate to the Controller menu. Press the ENT button to select the Controller menu.
  3. Navigate to the Network section of the Controller menu and press the ENT button. This takes you to the Network Parameters section.
  4. Navigate to Address and press the ENT button. The address defaults to 4.
  5. Press the ENT button. The address blinks.
  6. Use the up or down arrow to increase or decrease the address to the value you require. Press the ENT button.The address stops blinking and the display shows the old address.
  7. Press either the up or down arrow.The screen refreshes to the new address.
  8. Press ESC (Escape) to go back a single menu level. Keep pressing ESC and you return to the main screen that shows the system is operational.