Setting the VAC controller address using the Smart Building Hub - Verasys - LIT-12013067 - LC-VAC1000-0 - LC-VAC3000-0 - LC-IOM3711-0 - Field Device - Verasys Constant Volume Controller

Verasys Constant Volume Controller Application Note

Product
Controls > Field Controls > Verasys Constant Volume Controller
Document type
Application Note
Document number
LIT-12013067
Revision date
2023-04-27

Procedure

  1. Use the SBH to navigate to the VAC controller.
  2. Navigate to the Network section of the Controller menu to set the address.
    Note: The default address is 4; so if another controller conflicts with this address, disconnect the other address 4 from the trunk temporarily while you configure the controller or use the Setting the VAC controller address using the local display procedure.
  3. Click the Address field and use the up and down arrows to select the address you want to assign to the controller.
  4. Press Save.