You can add the LC-IOM3711-0 to the LC-VAC1000-0 or the LC-VAC3000-0 to increase the number of applications. For example, the LC-VAC3000-0 is a 32 point controller with all applications available on the base controller except for humidification, for which you must add the LC-IOM3711-0.
|
Feature |
Smart Equipment |
TEC3000 |
LC-VAC1000-0 |
LC-VAC3000-0 |
|---|---|---|---|---|
|
Up to two stage cooling |
Yes |
Yes |
Yes |
Yes |
|
Up to four stage cooling |
Yes |
No |
Yes |
Yes |
|
Proportional cooling |
No |
No |
Yes 1 |
Yes |
|
Proportional heating |
Yes |
No |
Yes |
Yes |
|
Up to two stage heating |
Yes |
Yes |
Yes |
Yes |
|
Up to three stage heating |
Yes |
No |
Yes1 |
Yes |
|
Heat pump |
Yes |
Yes |
Yes |
Yes |
|
Economizer |
Yes |
Yes |
Yes |
Yes |
|
Title 24 economizer Note: Title 24 sequence and alarm notification is implemented from
within the application. State of California certification is
pending.
|
Yes |
Yes |
Yes |
Yes |
|
Demand ventilation control |
Yes |
Yes |
Yes |
Yes |
|
Dehumidification |
Yes |
Yes |
Yes |
Yes |
|
Humidification |
No |
No |
Yes1 |
Yes1 |
|
Fixed variable fan |
Yes |
No |
Yes |
Yes |