Viewing BACnet devices in the SBH user interface - Verasys - LIT-12013606 - LC-SBH200-0 - BACnet integration - Verasys System - 4.0

Verasys BACnet MS/TP Integration Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
Technical Bulletin
Document number
LIT-12013606
Version
4.0
Revision date
2020-09-30
Product status
Active
A third-party device appears in the device list as displayed in the following image.
Figure 1. Third-party device in the device list

The following figure displays the default home page of a BACnet device.
Figure 2. Default home page of a BACnet device