Switching profiles for a BACnet device - Verasys - LIT-12013606 - LC-SBH200-0 - BACnet integration - Verasys System - 4.0

Verasys BACnet MS/TP Integration Technical Bulletin

Brand
Verasys
Product name
Verasys System
Document type
Technical Bulletin
Document number
LIT-12013606
Version
4.0
Revision date
2020-09-30
Product status
Active
Language
English

About this task

When you apply a profile, you lose all previous feature configurations that included the device. This includes alarm and trend data.

To switch profile for a BACnet device, complete the following steps:

Procedure

  1. Click on the device in the device list and navigate to the Profile view.
  2. Under the Configuration section, select the new profile that you want to use on the device and click Apply Profile.