Removing a profile from a BACnet device - Verasys - LIT-12013606 - LC-SBH200-0 - BACnet integration - Verasys System - 4.0

Verasys BACnet MS/TP Integration Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
Technical Bulletin
Document number
LIT-12013606
Version
4.0
Revision date
2020-09-30
Product status
Active

About this task

Removing a profile from a device removes it from all Verasys features.

To remove a profile from a BACnet device, complete the following steps:

Procedure

  1. Click on the device in the device list and navigate to the Profile view.
  2. Click the Reset to defaults button at the bottom of the page to disassociate the profile from the device and rediscover the device inside of Verasys.