BBMD settings - Verasys - LIT-12013606 - LC-SBH200-0 - BACnet integration - Verasys System - 4.0

Verasys BACnet MS/TP Integration Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
Technical Bulletin
Document number
LIT-12013606
Version
4.0
Revision date
2020-09-30
Product status
Active

Use BACnet IP Broadcast Management Device (BBMD) to set up the broadcast distribution table on the IP trunk. This feature allows for the SBH to communicate with an IP network that is located on a different physical subnet.

For information on how to set up the router feature for the BBMD, see Setting up router feature for BBMD.