BACnet controller integration overview - Verasys - LIT-12013606 - LC-SBH200-0 - BACnet integration - Verasys System - 4.0

Verasys BACnet MS/TP Integration Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
Technical Bulletin
Document number
LIT-12013606
Version
4.0
Revision date
2020-09-30
Product status
Active

As a BACnet integrator, the SBH monitors and supervises a network of BACnet devices and acts as a BACnet operator workstation for all integrated controllers. The devices page of the SBH presents data to the operator. You can add profiles to the third-party devices to show or hide data from views and to add extensions.

The following figure shows an example of how third-party BACnet devices can reside on the system bus alongside Smart Equipment controllers.

Figure 1. BACnet system integration configuration example