Premier RTU - Verasys - LIT-12013648 - LC-SBH200-0 - Building automation software - Verasys System - 4.0

Verasys Alarms Summary Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
Technical Bulletin
Document number
LIT-12013648
Version
4.0
Revision date
2021-04-01
Product status
Active
Table 1. Premier RTU Critical alarms summary
Description Cause
Circuit 1 locked out due to safety chain One of the safety chain switches opens three times.
Circuit 2 locked out due to safety chain
Circuit 1 locked out due to low pressure Low pressure switch trips three times in 120 minutes.
Circuit 2 locked out due to low pressure
C1A locked out due to high pressure HP switch trips three times in 120 minutes.
C1B locked out due to high pressure
C1C locked out due to high pressure
C2A locked out due to high pressure
C2B locked out due to high pressure
C2C locked out due to high pressure
C1A locked out due to low pressure
C1B locked out due to low pressure
C1C locked out due to low pressure
C2A locked out due to low pressure
C2B locked out due to low pressure
C2C locked out due to low pressure
Unit shutdown due to smoke A device in the shut down circuit opens.
Exhaust or return fan VFD failure Abnormal condition exists on the exhaust/ return fan VFD.
Supply fan VFD 1 failure Abnormal condition exists on the supply fan 1 VFD.
Supply fan VFD 2 failure Abnormal condition exists on the supply fan 2 VFD.
No heat/cool due to unreliable space temperature There is no reliable space temperature reference.
Option communication failure Loss of communication to options board. Check SA bus wiring and connections.
Building system interface board communication failure Loss of communication to building system interface board. Check SA bus wiring and connections.
Condenser 1 communication failure Loss of communication to refrigeration 1 board. Check SA bus wiring and connections.
Condenser 2 communication failure Loss of communication to refrigeration 2 board. Check SA bus wiring and connections.
Outputs disabled due to low input voltage Loss of 24 VAC power to 24 VAC OUTPUT terminal.
Outputs limited due to brownout input voltage Low voltage on 24 VAC OUTPUT terminal.
Cooling locked out - condensate overflow Check condensate drain for clogs.
Unit locked out due to high duct static pressure Duct static pressure (DSP) exceeds setpoint.
Unit locked out - airflow proof failure APS does not close when expected on fan start-up.
C1A locked out - exceeded operating envelope limits Variable speed drive compressor envelope control: This output shows lockout when three variable speed drive compressor operating envelope shutdown events occur within two hours of compressor runtime.
C1A locked out due to oil switch C1A oil switch open. Check crankcase oil level.
Furnace module 1 lockout Heating section 1 shutdown due to ignition control module. Check module for fault enumerator.
Furnace module 2 lockout Heating section 2 shutdown due to ignition control module. Check module for fault enumerator.
Furnace module 3 lockout Heating section 3 shutdown due to ignition control module. Check module for fault enumerator.
Table 2. Premier RTU Service Priority alarms summary
Description Cause
Unit shutdown airflow validation fail Heating and cooling shutdown, blower operation is not proven. Check APS, DSP.
Circuit 1 shutdown due to low pressure Low airflow, dirty filters, ice on coil, low charge.
Circuit 2 shutdown due to low pressure
C1A shutdown due to high pressure Dirty condenser coils, condenser fan failure, over charge.
C1B shutdown due to high pressure
C1C shutdown due to high pressure
C2A shutdown due to high pressure
C2B shutdown due to high pressure
C2C shutdown due to high pressure
C1A shutdown due to low pressure Low airflow, dirty filters, ice on coil, low charge.
C1B shutdown due to low pressure
C1C shutdown due to low pressure
C2A shutdown due to low pressure
C2B shutdown due to low pressure
C2C shutdown due to low pressure
HGRH locked out - valve stuck open Hot gas is flowing to reheat coil when no flow is expected.
HGRH locked out - valve stuck closed Hot gas is not flowing to reheat coil when flow is expected.
Main controller calibration error Cycle power to the unit. If error returns, contact technical support.
Option controller calibration error
Condenser 1 controller calibration error
Condenser 2 controller calibration error
Building system interface board controller calibration error
DAT sensor failure Sensor input out of expected range. Open or shorted circuit.
OAT sensor failure
RAT sensor failure
Building pressure sensor failure
Return fan pressure sensor failure
Evaporator coil temperature 1 sensor failure
C1A shutdown - exceeded operating envelope limits Variable speed drive compressor envelope control: This output shows disabled when a shutdown occurred due to the variable speed drive compressor exceeding its operating envelope limits. The compressor must remain off for 10 minutes.
Table 3. Premier RTU Service alarms summary
Description Cause
Circuit 1 shutdown due to safety chain One of the safety chain switches in circuit 1 opens.
Circuit 2 shutdown due to safety chain One of the safety chain switches in circuit 2 opens.
MAT sensor failure Sensor input out of expected range. Open or shorted circuit.
Outside air humidity sensor failure
Pre-filter pressure sensor failure
Final filter pressure sensor failure
Return air humidity sensor failure
Heat entering temperature sensor failure
Outside airflow sensor failure
Discharge air pressure sensor failure
Return air pressure sensor failure
Sensor calibration fault Sensor or sensors fails calibration test. Cycle power to unit. If error returns, contact technical support.
C1 liquid pressure sensor failure Sensor input out of expected range. Open or shorted circuit.
C2 liquid pressure sensor failure
C1 liquid temperature sensor failure
C2 liquid temperature sensor failure
C1 suction pressure sensor failure
C2 suction pressure sensor failure
C1 suction temperature sensor failure
C2 suction temperature sensor failure
Zone air humidity sensor failure
ZT sensor failure
OAQ sensor failure
Return air quality sensor failure
Discharge air humidity sensor failure
Exhaust heat recovery temp sensor fail
Slab humidity sensor failure
Slab temperature sensor failure
DAT cannot reach cooling setpoint Expected discharge air temperature does not occur due to high evaporator air temperature.
DAT cannot reach heating setpoint Expected discharge air temperature does not occur due to low evaporator air temperature.
Unit continuous runtime exceeds limit The AHU_AIRFDD_RunContinuous module is designed to alarm if the unit runs continuously beyond a defined time limit. The default is 23 hours. This means that the unit does not turn off by a time schedule. If the unit is designed to run continuously (such as a hospital), then adjust the alarm_delay to 0 in order to suppress the alarm.
Trim and respond not changing setpoint The AHU_AIRFDD_SPNotChanging module is designed to set an alarm if the setpoint input does not change in value during the alarm_delay interval. This is primarily used to make sure that the trim and respond setpoint adjust features are working properly. These features are usually in the supervisory controller.
Idle time while occupied exceeds limit The AHU_AIRFDD_UnitDownInOcc module is designed to set an alarm if the unit is shut down for a certain time period during the occ mode.
Economizer not economizing when it should Economizer damper does not open as commanded. Damper is stuck closed.
Economizer economizing when it should not Economizer damper does not close as commanded. Damper is stuck open.
Economizer damper not modulating Economizer damper does not respond to a change in the percent open or close command.
Excess outdoor air Too much outside air introduced into the unit. Outside air damper failure.
Space temperature cooling alarm Space temperature not at expected temperature within time period.
Space temperature heating alarm
Airflow detected without supply fan Airflow indicates when blower expected to be off. Check APS and/or Duct Static Pressure.
Unit has received a purge request Unit in a purge mode by a contact closure.
UV light needs service UV light module triggers this alarm.
Low OAT cooling cutout OAT is below the cooling lockout setpoint.
Heating locked out due to OAT OAT is above the heating lockout setpoint.
Hot water freezestat open to prevent coil freeze Air temperature at hot water heating coil is below setpoint.