Lighting Controller - Verasys - LIT-12013648 - LC-SBH200-0 - Building automation software - Verasys System - 4.0

Verasys Alarms Summary Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Verasys System
Document type
Technical Bulletin
Document number
LIT-12013648
Version
4.0
Revision date
2021-04-01
Product status
Active
Table 1. Lighting Controller Service alarms summary
Description Cause
Zone Select Alarm Circuit 1

Circuit has not been assigned a zone.

In the controller, define the number of lighting circuits and the number of lighting zones and then assign circuits to zones.

Zone Select Alarm Circuit 2
Zone Select Alarm Circuit 3
Zone Select Alarm Circuit 4
Zone Select Alarm Circuit 5
Zone Select Alarm Circuit 6
Zone Select Alarm Circuit 7
Zone Select Alarm Circuit 8
Zone Select Alarm Circuit 9