Access the remote access user portal and install the Airwall Agent - Verasys - LIT-12014321 - Network gateway - Airwall - 5.0

Verasys Airwall Agent for macOS Application Note

Brand
Verasys
Product name
Airwall
Document type
Application Note
Document number
LIT-12014321
Version
5.0
Revision date
2023-08-24
Product status
Active
Language
English

About this task

To set up the remote access user portal and install the Airwall Agent, complete the following steps:

Procedure

  1. From the remote access user portal, click Connect. See Figure 1.
    Figure 1. Remote access user portal home page
  2. From the pop-up window, click Mac Airwall. See Figure 2.
    Figure 2. Downloading Airwall Agent
  3. When the download completes, run as an administrator to install.
  4. When the installation completes, return to the remote access user portal and click Activate to auto-provision your Airwall Agent. See Figure 3. The provisioning process can take several minutes to complete.
    Figure 3. Initiate your activation code
  5. In the Open Airwall.app? pop-up window. Check Always allow cond-amera-01.openbluesec.cloud to open links of this type in the associated app and click Open Airwall.app.
  6. In the Airwall is trying to make network changes. pop-up, enter your Mac password.
  7. The installation is now complete but requires validation. Click the Airwall Agent icon from the Mac menu bar. See Figure 4
    Figure 4. Airwall Agent icon
  8. Click Configure.