The installation requires the set up of Okta multi-factor authentication and the installation of the Airwall Agent on your device. The Airwall Agent is automatically provisioned and managed by the Conductor. The Conductor is the central configuration and management point for your Airwall network and manages trust between the SBH300 and the Airwall Agent.
The installation consists of the following steps:
- Okta activation.
- Access the remote access user portal and install the Airwall Agent.
- Verify connectivity to the SBH300.