Access the remote access user portal and install the Airwall Agent - Verasys - LIT-12014323 - Network gateway - SBH300 Smart Building Hub - 5.0

Verasys Airwall Agent for iOS Application Note

Product
Document number
LIT-12014323
Version
5.0
Revision date
2023-08-24
Product status
Active

About this task

To set up the remote access user portal and install the Airwall Agent, complete the following steps:

Procedure

  1. From the remote access user portal, click Connect. See Figure 1.
    Figure 1. Remote access user portal home page
  2. From the pop-up window, click iOS Airwall. See Figure 2. This redirects you to the Apple App Store.
    Figure 2. Downloading Airwall Agent
  3. To download the Airwall Agent app, click Get.
  4. When the installation completes, return to your browser and click Activate to auto-provision your Airwall Agent. See Figure 3. The provisioning process can take several minutes to complete.
    Figure 3. Initiate your activation code
  5. When the provisioning is complete the Connected! icon appears. See Figure 4.
    Figure 4. Airwall connected
  6. Open the Airwall Agent app. From the Dashboard tab, turn on the Profile toggle switch.
  7. When prompted to authenticate, click JCI Okta.
  8. Enter your username and password. Click Next.
  9. Click Confirm remote session.