Airwall Agent configuration prerequisites - Verasys - LIT-12014322 - Network gateway - Airwall - 5.0

Verasys Airwall Agent for Android Application Note

Brand
Verasys
Product name
Airwall
Document type
Application Note
Document number
LIT-12014322
Version
5.0
Revision date
2023-08-24
Product status
Active
Language
English

Prepare your environment for the following items before you begin the installation of the Airwall Agent.

  • Android 6.0 (Marshmallow) and later.
  • Google account for Google Play┬« store.
  • SBH300 connected to a source of Internet. Refer to the Operation section of the Verasys Smart Building Hub (SBH300) Installation Guide LIT-12014293.

All external communications from the Airwall are limited to outbound ports TCP 8096 and UDP 10500, using the Host Identity Protocol (HIP) and must be open on the network. These ports are often closed in the networks of office buildings, university campuses, and other commercial sites. Consult with the IT department of the site to validate that the ports are open outbound. For Connected Verasys users, the cellular modem included with the SBH300 is pre-configured with ports TCP 8096 and UDP 10500 already open.