Wiring details - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document type
User Guide
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued
The wiring diagram describes the connections from the sensors to the HMS1655 backplane.
Note: Both the BAPI humidity sensor and Ashcroft® differential pressure transmitter receive power from the HMS1655 auxiliary power supply.

The fume hood controller model number is part code HMS1655. This model includes a controller module that mounts on the top of the monitored fume hood, and a mouted velocity sensor on the interior sidewall of the fume hood. The sidewall velocity sensor measures face velocities at the sash opening up to 200 ft/min with an accuracy of ±2 ft/min.

For a step-by-step procedure to configure the hardware resources of the HMS1655 fume hood controller for the application shown in Figure 1, see Configuring hardware resources.