Configuring the temperature sensor - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller
HMS1655 Fume Hood Controller User Guide
- Product
- Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
- Document number
- LIT-12014409
- Revision date
- 2024-05-27
- Product status
- Discontinued
Procedure
-
To configure the analog input resource for the input for the temperature sensor
of the combination sensor from BAPI (p/n BA/10K-2-H200-R), use the Analog Inputs
option on the first page of the System Setup menus.
-
Tap Analog Inputs Setup menus > Thermistor Input 1 to enter
the sash position sensor input configuration as follows:
- Thermistor Input: TI-1
- Thermistor Type: NTC Type 2
- Engineering Units: Degrees Fahrenheit
-
After you confirm the temperature configuration settings, accept the default
setpoint at the Enter TI-1 Setpoint configuration screen. If this controller
targets a temperature control application, configure this setpoint as required
by the specific application.