Configuring the sash position sensor - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

Procedure

  1. Use the Analog Inputs option to configure the analog input resource for the sash position sensor included with the HMS1655 fume hood controller, located on the first page of the System Setup menus.
  2. Tap Analog Inputs Setup menus > Analog Input 2 to enter the sash position sensor input configuration as follows:
    • Analog Input: AI-2
    • Engineering Units: in.
    • Input Range: 0V to 10V