Configuring the humidity sensor - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller
HMS1655 Fume Hood Controller User Guide
- Product
- Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
- Document number
- LIT-12014409
- Revision date
- 2024-05-27
- Product status
- Discontinued
Procedure
-
To configure the analog input resource for the relative humidity sensor input
of the combination sensor from BAPI (p/n BA/10K-2-H200-R), use the Analog Inputs
option on the first page of the System Setup menus.
-
Tap Analog Inputs Setup > Analog Input
3 to enter the sash position sensor input configuration as
follows:
- Analog Input: AI-3
- Linearization: Disabled
- Input Mode: Normal Mode
- Engineering Units: Percentage RH
- Input Range: 0V to 10V
-
After you confirm the humidity sensor settings, accept the default setpoint of
zero at the Enter AI-3 Setpoint configuration screen. If this controller targets
a humidity control application, configure this setpoint as required by the
specific application.