Configuring the humidity sensor - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document type
User Guide
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

Procedure

  1. To configure the analog input resource for the relative humidity sensor input of the combination sensor from BAPI (p/n BA/10K-2-H200-R), use the Analog Inputs option on the first page of the System Setup menus.
  2. Tap Analog Inputs Setup > Analog Input 3 to enter the sash position sensor input configuration as follows:
    • Analog Input: AI-3
    • Linearization: Disabled
    • Input Mode: Normal Mode
    • Engineering Units: Percentage RH
    • Input Range: 0V to 10V
  3. After you confirm the humidity sensor settings, accept the default setpoint of zero at the Enter AI-3 Setpoint configuration screen. If this controller targets a humidity control application, configure this setpoint as required by the specific application.