Configuring the flow sensor - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller
HMS1655 Fume Hood Controller User Guide
- Product
- Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
- Document number
- LIT-12014409
- Revision date
- 2024-05-27
- Product status
- Discontinued
Procedure
-
To configure the analog input resource for the flow input from the DP
transmitter (Ashcroft part no. CX-4-MB2-10-1IWL), use the Analog Inputs option
on the first page of the System Setup menus.
-
Tap Analog Inputs Setup menus > Analog Input 4 to enter the
sash position sensor input configuration as follows:
- Analog Input: AI-4
- Flow Range Maximum: 1 in.W.C
- Flow Range Minimum: 0 in.W.C
- Display Air Changes: No
- Input Range: 0V to 10V
- Duct Area: 28 in.2