Configuring the exhaust damper control - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller
HMS1655 Fume Hood Controller User Guide
- Product
- Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
- Document number
- LIT-12014409
- Revision date
- 2024-05-27
- Product status
- Discontinued
Procedure
-
To configure the analog output resource for the fume hood’s exhaust damper
control, tap Controller Setup > Analog
Output.
-
Input the sash position sensor configuration as follows:
- Analog Output: AO-1
- Operating Mode: PID Analog Output
- Output Range: 2V to 10V
- Maximum Limit: 100 percent
- Minimum Limit: 0%
- Input Channel: AI-1
- Action Mode: Reverse