Configuring the display settings - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

About this task

Figure 1. Comprehensive wiring

Procedure

  1. To save the setting to non-volatile memory, tap Display Setup menus > Display Modes > Single Sensor Mode > OK.
  2. To specify the sources for the sash position and temperature to display on the main screen, tap Display Setup menus > Display Modes > Set Display Options and select all four display options.
  3. To specify the sources for the individual sensors, tap Next.
  4. Configure the sources as follows:
    • Sash Position Source: Analog Input 2
    • Temperature Display Source: Thermistor Input 1
  5. To save the setting to non-volatile memory, tap Finish.
    Note: Since this fume hood controller monitors and controls the face velocity at one sash opening, select the display mode to support a single sensor fume hood controller.