Configuring sidewall velocity sensor settings - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

On the first page of the Controller Setup menu you can confirm the sidewall velocity sensor configuration settings. Configure the sidewall-mounted velocity sensor included with the HMS1655 fume hood controller as follows:

  • Analog Input: AI-1
  • Linearization: Enabled
  • Input Mode: Normal Mode
  • Engineering Units: Ft/min
  • Input Range: 0V to 5V