Configuring hardware resources - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

To configure the HMS1655 fume hood controller for the application, as shown in Figure 1, set up of the sidewall velocity sensor, temperature sensor, humidity sensor, flow sensor (DP transmitter), and display configuration. The sidewall-mounted velocity sensor is configured and calibrated at the factory and is not adjustable. To field calibrate the sensor after installation in the fume hood, complete the following: