Configuring analog outputs - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

You can use the fume hood controller to monitor and control the face velocity at the sash opening. Therefore, you can use the analog output AO-1 to control the associated exhaust damper, operate in closed-loop or PID control mode, and output a 2 VDC to 10 VDC signal to the controlled damper actuator.