You can use the fume hood controller to monitor and control the face velocity at the sash opening. Therefore, you can use the analog output AO-1 to control the associated exhaust damper, operate in closed-loop or PID control mode, and output a 2 VDC to 10 VDC signal to the controlled damper actuator.