Setting up analog inputs for monitoring sash position - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

About this task

You can configure the HMS1655 monitor and display sash position or height in real-time with the sash position sensor (part no. POS-100).

Procedure

  1. To configure one of the secondary analog inputs to monitor the sash position from the Select Input Type configuration screen, tap Sash Position > Next.
  2. The Analog Input Settings configuration screen appears. You can select the engineering units, voltage, or current input range for the connected sensor.