About this task
Procedure
- To configure one of the secondary analog inputs for humidity measurement from the Select Input Type configuration screen, tap Humidity > Next. The Analog Input x Settings configuration screen appears. You can select the engineering units, voltage, or current input range for the connected sensor.
- If you use the humidity input for a humidity control scheme, tap Next at the popup to open the Setpoint Entry Configuration screen where you can enter a target humidity setpoint.
- Map the humidity input to one of the analog outputs configured for PID control mode.