Remapping the secondary analog outputs - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

You can remap each of the analog outputs at the final configuration popup, or remap them with the Analog I/O Mapping option on the Analog Inputs Setup menus. This option opens the Analog I/O Mapping configuration popup.

You can map each analog output to one of the analog input resources, including the two dedicated thermistor inputs. If you select a different analog input channel for any given analog output, the existing mapping for that output is canceled. However, you can map multiple analog outputs to the same analog input, which can each have their own specific setpoints associated for their particular application.