Deleting an existing password - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document type
User Guide
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

Procedure

  1. To delete an existing password entry, enter the password to be deleted into the user menu system.
  2. Tap Delete Password on the Password Setup menu, and tap OK to confirm that you want to delete the existing password.