Managing system passwords - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

The HMS1655 fume hood controller incorporates a system security password facility to prevent unauthorized access to the system menus and configuration settings. The password facility has a capacity of 10 unique, multiple access level passwords.

To add and delete entries from the system, use the password setup option.