Enabling individual audible alarms - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

About this task

You can individually enable each of the universal analog inputs and the two dedicated thermistor inputs audible alarming.

Procedure

  1. To open the Alarm Buzzer Settings configuration popup from the Alarms Setup menu, tap Audible Alert.
  2. After you select the individual analog and thermistor inputs, which activate the audible alert when in alarm mode, tap Next to open the Alarm Buzzer Settings configuration popup.
    Note: You can select the alarm buzzer for one of two modes of operation: Audible Mode or Silent Mode.
  3. If you select audible mode, enter the desired delay in seconds or minutes. To specify the Alarm Quiet Period of the audible alarm buzzer in audible mode, tap Next to open the Alarm Buzzer Settings configuration screen.
  4. If you select silent mode, the alarm buzzer does not sound whenever the enabled analog inputs enter alarm status.