About this task
- If you select Timer-Based mode as the trigger mode for the relay output, enter
for the acting mode and the activation duration associated with the alarm relay.
Note: This trigger mode only activates the alarm relay if the corresponding analog input is configured for Sash Position and the specified duration timer has expired.
For more information on the options available on the PID Loop Setup menu and the configuration of the secondary PID loops on the HMS1655, see Configuring secondary PID loops.