Configuring setpoints mode - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document type
User Guide
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

About this task

Setpoints mode uses a pair of setpoints that correspond to the mapped analog input to determine when to activate or deactivate the relay output.

Procedure

  1. If you select Setpoints Mode as the trigger mode for the relay output, enter a high setpoint and a low setpoint. The high setpoint determines the threshold at which the relay output activates if in direct acting mode, or deactivates if in reverse acting mode. The low setpoint determines the threshold at which the relay output deactivates if in direct acting mode, or activates if in reverse acting mode.
  2. After specification of the high and low setpoints, enter the acting mode and delay associated with the relay output.
  3. In direct acting mode, the relay output activates when the sensor input exceeds the high setpoint, and deactivates when the sensor input falls below the low setpoint.
  4. In reverse acting mode, the relay output deactivates when the sensor input exceeds the high setpoint, and activates when the sensor input falls below the low setpoint. The relay output delay is a maximum of three minutes in duration.