Configuring secondary relay outputs - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

You can use the Relay Setup menu to configure the secondary relay outputs as required by the specific application. Select one of the relays on this menu to open the Relay x Trigger Mode configuration screen. You can configure the selected relay output to trigger with one of three methods: Setpoints, Operating Mode, and Timer-Based.