About this task
Procedure
- To specify the proportional, integral, and derivative constants used by the closed-loop control scheme for the corresponding analog output, click one of the secondary PID loops from the PID Loop Setup menu to open the PID Loop x Settings configuration popup menu.
- You can adjust the three dimensionless PID constants from 0 to 100 with the three sliders on the configuration screen.
- See the Alarms Setup menu and the configuration of the alarm resources on the HMS1655 for more information.