The System Setup menus support configuration of all the HMS1655 hardware resources. The first page of the System Setup menu provides configuration options for the four universal analog inputs, two thermistor inputs, four digital inputs, and four relay outputs.
The second page of the System Setup menu provides configuration options for the four PID loop settings, all of the alarm settings, specification of the engineering units for each analog input, and system security password management. Several of the configuration options on the System Setup menus, specific to the hardware resources, are redundant with those on the Controller Setup menus.