Setting up the main sensor input - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document type
User Guide
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

About this task

The Analog Input option on the Controller Setup menus enables configuration of the sidewall sensor input as required by the specific application. This option opens the Sidewall Sensor Settings configuration screen. At this configuration screen, you can specify whether or not to enable the linearization of the sensor input, and whether or not to invert the analog input signal. The Inverted Mode option is useful if the actual sidewall sensor connected to the HMS1655 was inadvertently installed backwards and if the reference and monitor ports of the velocity sensor are reversed. The Inverted Mode is equivalent to the manual reversal of the installation orientation of the sidewall sensor assembly.
Figure 1. Sidewall sensor settings configuration

Procedure

  1. To open the Sidewall Sensor Settings configuration screen, tap Next.
  2. You can select the engineering units, the voltage, or the current range for the sensor input. The sidewall sensor input defaults to the 0 V to 5 V range. To open the Enter Occupied Setpoint configuration screen, tap Next.