Configuring target setpoints - Triatek - LIT-12014409 - HMS1655 Fume Hood Controller

HMS1655 Fume Hood Controller User Guide

Product
Controls > Fume Hood Controls > HMS1655 Fume Hood Controller
Document number
LIT-12014409
Revision date
2024-05-27
Product status
Discontinued

About this task

The Edit Setpoints option on the Fume Hood Setup menu opens a popup numeric keypad where you can enter a new setpoint for the selected operating mode. For example, if the HMS1655 is in Occupied operating mode, you can use the Edit Setpoints option to enter a new face velocity setpoint for Occupied mode.

Procedure

  1. To enter setpoints for the other operating modes, select the mode from the Operating Mode popup screen.
  2. Tap Edit Setpoints to enter the target setpoint for the selected mode. The default setpoints for Occupied, Unoccupied, and Decommissioned mode are 100 ft/min, 60 ft/min, and 40 ft/min, respectively.