About this task
The Edit Setpoints option on the Fume Hood Setup menu opens a popup numeric keypad where you can enter a new setpoint for the selected operating mode. For example, if the HMS1655 is in Occupied operating mode, you can use the Edit Setpoints option to enter a new face velocity setpoint for Occupied mode.
Procedure
- To enter setpoints for the other operating modes, select the mode from the Operating Mode popup screen.
- Tap Edit Setpoints to enter the target setpoint for the selected mode. The default setpoints for Occupied, Unoccupied, and Decommissioned mode are 100 ft/min, 60 ft/min, and 40 ft/min, respectively.